Other Parts Discussed in Thread: LM321
Hi,
I am using a TPS24720 as a efuse for 12V, 10.9A. Using the spreadsheet tool for this part, i have come up with the following values:
Rsense = 2mohm
Rset = 44.2ohm
Rimon = 1.37Kohm
One of the useful features of the TPS24720 is the Imon output which i am feeding into a LM321 op amp with a gain of 4.01 which is then feed into a ADC to monitor the current that is being passed through the TPS24720. What i am seeing now is that the measured voltage on the Imon pin does not match my calculations of what the current should be. In the lab i have tested with the following conditions:
Vin = 12V
I = 2.47A
Vimon = 183mV (measured)
Based on the selected resistors, i get a calculated value of 153mV for Vimon. I repeated this test with the op amp disconnected from Imon and i get measure the same Vimon value. What am i doing incorrectly here as the measured and the calculated value is off by a lot.
Thanks