Hello,
I have a design using the LM25066.
When I read the temperature values the results are very noisy. (Varying from 21 to 28 degC)
I get similar noise when reading power and current values - even when I read the averaging registers.
The device is located between two switching power supplies - so perhaps it is picking up noise from those?
Do you have any advice?
For example, I have used a 1nF cap on the input to the DIODE pin. Would it be sensible to increase that capacitance?
Thanks, Fiona