Guys, I am working with a customer and have the following question on layout for the LMZM33603.
The layout and pin descriptions say to keep AGND (zero reference) separate from PGND (power ground) on the LMZM33603. Recommendation is NOT connect them together. BTW, this board also has an LMZ34002RKG on it.
In the design, everything is referenced back to the input supply (24V wall wart) and chassis. I think we can keep AGND isolated from PGND immediately in the vicinity of the LMZM33603, by putting a route obstruct between those planes. this should help define return paths, but I don’t know if that’s adequate, because AGND and PGND do end up getting connected at the main supply a couple inches away. ATTACHED image has a rough idea of what the design will look like.
Questions:
1. Is this a big deal and how will it impact my performance?
2. Do you have guidance for using the LMZM33603 if it is not feasible to have isolated AGND and PGND planes?