Hi guys,
My customer approached me with the below question:
We recently have a DC-DC isolated converter project in which we would like to consider the TI Buck regulator LM5017 to generate internal voltage source to power the PWM controller and drive MOSFETs. We refer to the schematic in LM5017 data sheet Figure 17, page 19 . The input range and output voltages are listed below for consideration:
Vin=7.5 – 18V
Vout1=6V
Vout2=11.5V
Total power less than 3W
The design note 8.2.2.2.1 states that “The primary output voltage is normally selected based on the input voltage range such that the duty cycle of the converter does not exceed 50% at the minimum input voltage. This condition is satisfied if VOUT1 < VIN_MIN / 2.” Why this buck regulator with isolated output requires 50% max duty ratio? (Single output shown in Figure 13 doesn’t have such limitation.)
In our case, if we need 6V at the primary. If we set this output as regulated output, the max. duty ratio would be 0.8. It seems we have to consider an artificial lower voltage output, saying 3V, as regulation target to satisfy such requirement. Is this the way to avoid duty ratio running into >50%?
Now, I found an app note that mentions this requirement is because "the isolated outputs only have the off-time window to transfer energy, for a duty cycle that is too high, the secondary winding current will have a huge spike, which leads to poor regulation."
Is it ok to break the 50% rule if you don't need very good regulation on the isolated rail? Could you put an LDO on the output of that isolated rail to smooth it out if needed?
Thanks,
Brian