hi team,
how to know the highside mosfet voltage withstand? Whether it has risks based on the SW waveform? (The input is 12v) Need us to use the full bandwidth of the probe? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi team,
how to know the highside mosfet voltage withstand? Whether it has risks based on the SW waveform? (The input is 12v) Need us to use the full bandwidth of the probe? Thanks.
Frank,
Generally you can look at the absolute maximum rating for the SW node in the datasheet, section 6.1 for TPS56121. The actual breakdown voltage will be somewhat higher, but it is guaranteed up to the abs max limit, which is 25 V for TPS56121.
Frank,
I would use the highest BW available or better yet a differential probe. If using a regular probe make sure to keep the ground loop as short as possible (< 1cm). The worst case stress for the high side FET is on the falling edge of the SW waveform when the high side turns off and the negative SW node transient occurs. VIN minus the transient undershoot voltage is the voltage across the high side FET. It should be less than 25 V.