Part Number: UCC28251
Other Parts Discussed in Thread: UCC2897A
Dear All,
i approached to a hard switching topology for a wide range duty cycle application in several posts.
i selected the half bridge working with UCC28251.
the output voltage range is 0 to 40 V ( adjustable ).
the input voltage is 400 V ( form UCC28019A PFC stage ).
the maximum current is 10 A and the load is a resistance ( variable resistance 400 W ).
please see the bellow schematics ( form data sheet ):
there is a ordinary transistor output optocoupler in the "feedback and isolation" block.
i have two questions:
1) can optocoupler work for the complete/wide range output voltage? in other words; is there linearity problem with such an output voltage range from 0 to 40V?
2) should i to worry about flux walking of the half bridge topology in voltage mode control?
Best Regards,
Ras