Hi,
my customer would like to measure the bode plot of current loop of UCC28070 with loop analyzer.
But how could it be accomplished?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
my customer would like to measure the bode plot of current loop of UCC28070 with loop analyzer.
But how could it be accomplished?
PFC_LoopResponse.pdfHello Howard,
The method for measuring loop response is detailed in the attached TI seminar document.
Special conditions relating to the high output voltage are described in page 29
Regards
John
Since UCC28070 do not sample PFC inductor current directly, and only sampling mos current to do the control. Can you advise customer to add a small resistor, for example, 10ohm between pin CSB and the negative pole of diode on the CT sampling circuit?
I think it may be ok to do the current loop test at this point, and please make sure the GND should be connected to the same GND point of UCC28070.
I attached the test point here.
Hi David,
Have you ever used this method to measure the current loop of UCC28070? The CSB test the MOSFET current, this current should be discrete. If add a disturbance here, can the circuit work well and show the correct Bode diagram?
Regards,
Lenna