Other Parts Discussed in Thread: LMZ34202
Hello,
Can I drive short (~ 100us) load current pulses higher than 1A max output current? I would expect about 1.2A to 1.3A peak current.
Will LMZM23601 operate in current limiting (1A) mode in this case and peak currents will be handled by the output capacitor. If 5V output LMZM23601 connected to 4 Ohm load will it operate in current source (current limit mode) and drive 4 Ohm resistor with 1A current?
Thank you!