This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40425: May tps40425 can support Vout ramp time?

Part Number: TPS40425

Hi Sir 

My customer device request ramp time as below. May TPS40425 can support?  

Condition TPS40425 Vin is 12V vout is 3.3V @0.66ms~10ms and 0.8V@ 0.05ms ~10ms.

If yes, how to set up in circuit? or here have other suggestion solution?

PS: Vout load are 0.8V/18.85A and 3.3V/49.9A

                                        Bogey

  • Hi Bogey,

    The PMBus register TON_RISE (61h) can be used to set soft-start time.

    The soft-start time can be programmed from 0.6ms to 9ms.

    You also can use TI Fusion to set soft-start time easily.

    Thanks

    Qian

  • Hi Qian

    More few questions,

    1. Can you told me the default soft-star timing ?

    2. How to use TI Fusion to set the soft-star timing?

    3. If the timing can’t meet the requirement, we should be follow the below flow. Right?

     

    Power up 12V feed to VDD of TPS40425à Program register TON_RISE(61h) to the soft star is around 2msàenable TPS40425

     

    1. We only connect the CNTL1 for enable function, right?

  • Hi Bogey,



    1.Can you told me the default soft-star timing ?
    The defualt setting is 2.7ms.

    2.How to use TI Fusion to set the soft-star timing?
    It is in Fusion->Configure.
    If you installed Fusion, you will find it.

    3.If the timing can’t meet the requirement, we should be follow the below flow. Right?
    The time information on your pictur is not clear. Is there a delay time between two rails?

    Thanks
    Qian