This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2330: TPS2330 as a power switch

Part Number: TPS2330

I’m attempting to use the TPS2330 as a power switch. I have a 12V battery-powered system. I want to control the overall power (about 3A) on/off by toggling the enable pin the TPS2330. Then, I want to do the same on another current leg (about 1A) of the system downstream from the overall power. I’m having trouble getting this to work. Has anyone done any similar application with this device?