In my circuit, I generate 4.2 V from 12 V, but there is no time delay of 1 ms.
In the waveform, VIN <3.5 V, so I think UVLO is operating.
Therefore, I think that it will be output 1 ms later when VIN> 4.0 V, but there is no delay.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In my circuit, I generate 4.2 V from 12 V, but there is no time delay of 1 ms.
In the waveform, VIN <3.5 V, so I think UVLO is operating.
Therefore, I think that it will be output 1 ms later when VIN> 4.0 V, but there is no delay.
I retested Vin so that it is lower voltage.
When Vin becomes sufficiently low, output delay occurs.
Therefore, in the case of the attached waveform, UVLO does not appear to be functioning.
However, since the voltage of EN is over 1.0 V, I thought that we will start outputting at an earlier timing, but it will not be output.
When Vin is 4 V or less, will not we start outputting in any case?
Best Regards,
Thank you for your reply.
I understood that both EN> 1.0 V and VIN> 4.0 V are required for the output, and also UVLO is need a little time for detect.
Therefore, I'm thinking that the waveform I uploaded does not satisfy that specifications.
So I think in this situation, the output does not delay.
Best regards,