Other Parts Discussed in Thread: BQ77905, , LM5060-Q1, LM5060
Hi all,
my requirement is to use an OVP circuit, to prevent from the customer to insert the wrong charger.
I was planning to use the LM9061 together with a battery pack (with BQ77905 chip set).
I know the battery has an OVP circuit, but the requirement is to prevent it from even "seeing" the battery.
I was expecting that the LM9061, connected as my schematics shows, will see that the voltage is higher than 25V, and won't drive the output.
instead it allows any voltage to drive Q14.
can you see why?
I thought that the ON/OFF pin should keep the output disconnected, until an input between 7V~23.5V is inserted, only then it will drive Q14.
when Q14 is open, the battery forces a voltage which is under between 15V to 21V - but that should happen only after the charger insertion and opening of Q14.
regards,
Ran Aloni