Dear TI Support,
Attached is a schematic drawing showing three (3) power supplies, each designed around the TPS54020 switching regulator.
The design team no longer exists and I’m trying to reverse engineer this design to see that it satisfies the requirements of the TPS54020.
A timing diagram is shown on the drawing which indicates Turn ON voltage and Coincidental Tracking.
I have a few questions about this design and was hoping TI could provide some recommendations and guidance.
My first question relates to the ON/OFF Threshold specified by the resistor divider of R3 & R5. Each supply has identical thresholds.
According to the datasheet, “To achieve clean transitions between the OFF and ON states, TI recommends that the turn OFF threshold is no less than 4.2 V, and the turn ON threshold is no less than 4.4 V on the VIN pin.”
Since the OFF & ON trip points are 4.2V and 4.4V (rounded), there is no margin. Additionally, the Main +5.0V input can range from +4.634V to +5.234V.
Secondly, I remain confused about how to calculate the Tracking resistors.
Based on the attached design, I cannot figure out how ΔV was calculated and if the selected resistors meet the design requirements.
Additionally, can you explain what the SS input threshold is that turns ON the part.
I clearly don’t understand this specification;
From a new design perspective, what would be the correct design steps for coincidental tracking. How does one arbitrarily choose values for VOUT1 and VOUT2, then guarantee that value of RS1 is satisfied.
From the datasheet “The ΔV variable is zero volts for simultaneous sequencing.” Well, if ΔV = 0V, then RS1 computes to 0Ω, and RS1 fails to meet the requirements of “RS1 > 2800 ´ VOUT1 -180 x ΔV”
So, based on the information provided, any assistance, explanation, and guidance you can provide is GREATLY appreciation.
Thanks so much!
Best regards,
Barry Weinberger
Barry Weinberger
Sr. Hardware Engineer
Curtiss-Wright
20130 Lakeview Center Plaza, Suite 200, Ashburn, VA 20147
T: 703-840-6727
bweinberger@curtisswright.com | www.curtisswrightds.com