Part Number: TPS63070
Other Parts Discussed in Thread: TPS63020
Hi All,
I'm designing a buck/boost and the TPS63070 looks like it will meet the spec. I have to carefully budget the system quiescent current, as it is a very tough to meet low power specification. Quoting from the datasheet -
| IQ | Quiescent current | into VIN; IOUT= 0 mA, VEN = VIN = 6 V, PFM VOUT = 5 V; Tj = -40°C to 85°C |
54 | 103 | μA | |
| IQ | Quiescent current | into VIN; IOUT= 0 mA, VEN = VIN = 6 V, PFM VOUT = 5 V; Tj = -40°C to 125°C |
133 | μA | ||
| IQ | Quiescent current | into VOUT; IOUT= 0 mA, VEN = VIN = 6 V, VOUT = 5 V, PFM Tj = -40°C to 85°C |
5 | 9 | μA | |
| IQ | Quiescent current | into VOUT; IOUT= 0 mA, VEN = VIN = 6 V, VOUT = 5 V, PFM Tj = -40°C to 125°C |
17 | μA | ||
| ISD | Shutdown current | VEN = 0 V; Tj = -40°C to 85°C; VIN = 5V |
2 | 12 | μA | |
| ISD | Shutdown current | VEN = 0 V; Tj = -40°C to 85°C | 26 | μA |
What does "into VOUT" mean please? Putting power or voltage back into the device at Vout doesn't seem like a good idea to me! At least according to all buck/boost topologies from books.
The quiescent current with 5V fed into Vout is much less than with the chip in shutdown.
Please can anyone clarify, and pass along any tips on minimising current when the chip is in shutdown?
Regards,
Rob.