Part Number: LM5022
Other Parts Discussed in Thread: LM5155, TIDA-020009
Team,
I have seen the below LM5022 TI design for a BUCK/BOOST based on SEPIC:
http://www.ti.com/tool/PMP40488
-Are we planning any SEPIC TI design based on LM5155?
-What would be the methodology to dimension the below system?
Vin: 12V
2V < Vout < 48V
I out max < 0.5A
The design need to be flexible enough to accommodate this wide Vout range even if the efficiency is not optimum.
-Webench enables to simulate either BUCK or BOOST but not both. Also LM5155 has only a "Quick start calculator" for BOOST.
What would be the best approach to make a quick evaluation for the above specs?
Thanks in advance,
A.