Other Parts Discussed in Thread: BQ35100, , BQSTUDIO, EV2400
Hello,
We have implanted BQ35100 on a board for LiMnO2 battery gauging (CR2 and CR123A).
The board is operational but the value recorded with BQ35100 do not seem correct.
So we have purchased BQ35100EVM-795 and EV2300 to run separate tests using BQ Studio.
We have several problems:
1. After installation of BQ Studio, you give a procedure for installing the specific driver of EV2300 in the document SLUUBH7.pdf (''bq35100EVM-795 Evaluation Module'').
''If the EV2300 is connected, wait until the system prompt New Hardware Found appears.
Choose Select Location Manually, and use the Browse button to point to subdirectory TIUSBWin2K-XP-1.''
We could not locate this subdirectory and the installation finished without proper installation of the driver.
As a result the EVM2300 is seen as ''unknown peripheral'' in Windows Peripheral Manager.
=> Where can we find the driver and can it be installed through the peripheral Manager?
2. When starting BQ Studio and selecting ''Gauge'' and then ''0100-1-02_bq35100.bqz'', a window opens (see picture) saying that the device is not compatible with the application.
Thanks for any help to complete installation of EV2300 and to start using our EVB.
Software versions:
- Windows version: Windows 10 64-bit
- Battery Management Studio ( bqStudio ) Version : 1.3.86 Build Date : June 8, 2018
Best regards,
Olivier