This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

UCC28780EVM-002: Simulation (Spice model of UCC28780 and UCC24612)

Prodigy 30 points

Replies: 5

Views: 585

Part Number: UCC28780EVM-002

Dear Sir

I would like to make a transient simulation of the UCC28780 Active Clamp Flyback 45W AC/DC EVM with GaN FET. I see that only Simplis Model of the UCC28780 and UCC24612 are available.

Could you provide the spice model of the UCC28780 and UCC24612 in order to make a LTSPice Simulation or the only way is to do a simulation using Simplis?

Thanks

Best regards,

Nicola

  • Nicola

    We only have a SIMPLIS model available for UCC28780. There is no spice model.

    UCC28780 is very complicated, which will make it a challenge to simulate in spice. As a result we have released a model in SIMPLIS, which is a simulation tool that is optimized for switched mode power supply design.

    Best Regards,
    Eric
  • Dear Eric,

    thank you for your response!

    Could you provide the PCB layout file of the UCC28780EVM-002 for reference (like CAD file)?

    I'd like to refer the layout and try to realize the PCB by myself in order to practise.

    Thanks

    Best regards

    Nicola

  • In reply to Nicola Bigoni:

    Nicola

    UCC28780EVM-002 was developed in Altium.  Attached are the Altium files and gerber files for this design.

    Best Regards,

    Eric

    HVP002A_Gerbers.zip

    HVP002.zip

  • In reply to Eric Faraci:

    Dear Eric,

    I'm able to open the schematic files from the design files but not the PCB project.

    I'm using Altium 2018.

    Please let me know

    Best regards

    Nicola

  • In reply to Nicola Bigoni:

    Nicola

    I am able to open the Altium project file HVP002.PrjPcb, then thru it open the schematic HVP002A_p1.SchDoc, HVP002A_p2.SchDoc and HVP002A_Hardware.SchDoc and PCB file HVP002A.PcbDoc. I have Altium 18.1.9 on my computer.

    Can you let me know what error you are seeing?

    Best Regards,
    Eric

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.