Other Parts Discussed in Thread: EM1402EVM, EMB1499Q
Hi,
I have EM1402EVM and i want to get 1st test so can i use BQ76PL455Q1EVM GUI for test?
Thanks and regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have EM1402EVM and i want to get 1st test so can i use BQ76PL455Q1EVM GUI for test?
Thanks and regards,
Yes votages are right i can see serial port in device manager and port is opening in real term terminal but not in bq76pl. I have seen some comments on community and most of the people facing the same issue. Please help us to find solution.
Hi Taylor,
As you said i checked possibilities,
Can you verify that you downloaded the correct 32 bit or 64 bit version?
i downloaded from GUI from http://www.ti.com/tool/bq76pl455evm-gui-sw?jktype=recommendedresults and downloaded USB to TTL driver from link you given
Did you verify checking other cables?
Dirver successfully updated and can see port 3 and its working fine, i did verify with short TX RX and typing and receiving on Real Term so it is working.
Can you confirm that nothing else is using the COM port? (Teraterm/realterm/serial port)
Yea no other software is using serial port
Can you check with a different USB port and another Windows PC/OS?
I tried with other ports and other PCs with windows 7, windows 8.1. still its giving unable to open port.
I just connected USB to serial and this is only power source to the board. VIO = 5.3 V and VP = 1.8 V and VDIG = 1.8 V. I have not connected Cells or 12 V supply. I read VDIG should be 5.3 V and its getting 5.3 V from cells supply, is it right? whats the problem here to not opening port? am i need to connect cells there? to open your GUI?
Hi Taylor,
Yea after connecting cells its opened but is not balancing. I connected 6 cells and remaining pins i short with pin16. so is showing voltage in cells tab of every cell. When i am start balance between 2 cells cell 1 and cell 2 having voltages 3.85v and 3.75 respectively. i wait for 35 minutes but they were not balanced. What is the balancing current, can i control? I am using 3.7v and 2000mAh cells. Is it possible with GUI and EM1402EVM? or i have to use example code?
I think we got the problem as it is active system we will need TMS570 launch pad with example code connected to BMS board and that launch pad connected to PC through USB. That way it will, I will check that. I am not understanding how balancing is going on here? I was reading documentation "TMS570 Active cell balancing battery management design guide" I am little confused with some lines. Check attachment for snap of it.