This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: UCC39002 + PMP5236 - Power supply unstable at low load

Part Number: UCC39002

My customer is working a dual POE power supply based on UCC39002 and PMP5236.

So far , the problem is that the power supply oscillates between 2 power rails at light load and stops oscillating when the load goes up to 120mA.

Once the oscillating stopped, the circuit can work on a 30mA load with current balancing.

Could you help solve this issue?