This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5141-Q1: LM5141-Q1 EVM, how to select D1 and D2

Part Number: LM5141-Q1

Dear TI:

   How to select the D1 and D2?  The schematic is from LM5141EVM, my application is 12V->5V/10A:

   I want to select D1 and D2, Which parameters do I need to focus on?

Thanks!

  • Hi Eric,

    D2 only conducts during the deadtime (the current commutation from the low-side FET's body diode to the antiparallel Schottky is highly dependent on inductive parasitics, so most of the current doesn't commutate if the deadtime is < 20ns). I think D1 is not required given the short deadtime of the LM5141-Q1, particularly if the low-side FET's body diode has a reasonable Qrr. Note also that D2 adds SW node parasitic capacitance, so it can reduce light-load efficiency when operating in CCM.

    D1 is the boot diode that charges the boot cap - it should be rated for greater than the input voltage and typically more than 100mA. Usually, it's a Schottky diode to achieve low forward voltage drop, but also beware of possibly high reverse leakage current at high temperatures. A small SOD523 or SOD 323 package is adequate.

    Regards,
    Tim

  • Dear Tim:

        Thanks very much!

    Regards!

    Eric Shen