The REF5030 (or any of these REF50xx devices) state to use a 1-50uF output cap, connected from Vout to GND.
If i use a 10uF cap at the output pin, can this part support additional capacitance if it's not located directly at the output pin? I have an application where I need to have this reference in multiple locations around my design, so trace and additional local bulk capacitance could be present. I want to make sure it won't cause this part issues. I don't see a statement anywhere saying a maximim capacitance value. If this is ok, are there still ESR requirements for each cap location?
Thanks.