I have a question about TPS 51200.
For details, please see the attached file.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Thank you for your reply.
Load current: DDR: 0.6 A
The current of VO was measured. There is inrush current as 2A. (Attachment)
For the capacitor of waveform 3, it is OK.
I have an additional question.
For details, please see the attached document.
Thank you.
Masazumi-san,
The VLDOIN current is equal to "Cout charging current" + "output current". The Cout charging current is the current charging Cout when Vout rises up.
In your measurement, the VLDOIN current is 2A, output current is 0.5A, and Cout Charging current is 1.5A.
Thanks
Qian
Hello.
Thank you for your answer.
The current of VTT is measured near VO pin of TPS51200. It is between electrolytic capacitor and Vo pin.
I think that the charging current of capacitor + load current = 0.5 A (peak). (I think this state)
For details, please see the attached document.
Thank you.