Other Parts Discussed in Thread: PMP11254,
Please let me confirm about my understand is correct or not for PoE standard.
Information of PoE standard is attached below, is this mean ① and ② correct?
①Over current
When overload current (Icut) continue to flow on the time of Overload time limit (Tcut, 50ms~75ms), PSE will be off the power source.
②Short condition
When short current (Ilim) continue to flow on the time of Short circuit time limit (Tlim, 10ms~ at Type-2), PSE will be off the power source.
Customer is evaluating TPS23751 based on PMP11254 and below condition (No load).
・Connect LAN to PSE ⇒ After PSE sequence, supply PSE to VDD(52V) ⇒ VDD supply to VC ⇒ When TPS23751 startup, inlush is occur
Customer want to confirm below inlush is keep the rule of PoE standard or not.
Best regards,
Satoshi