Hi TI,
I am trying to use the BQ24725A in a lower cost battery charger design. Since our charging current is low(190mA), we used a relatively large sensing resister(0.15) at the output. Now it seems the output voltage(1.32V) is lower what we set(8.4V) through I2C, could you help to check?
BTW, I have jumped the pin CMSRC to VCC input(9V25), but I don’t know why I need to do that, because in the block diagram, this pin provides the base power for the voltage pumper of ACDRV.
Please check the schematic below:
The register setting is listed below:
0x12 0x0030 (option register)
0x14 0x0c00(charge current)
0x15 0x20c0(charge voltage)
0x3f 0x1000(input current)
Thanks so much!
Best Regards,