Part Number: BQ24725A
Hi TI,
I am trying to use the BQ24725A in a lower cost battery charger design. Since our charging current is low(190mA), we used a relatively large sensing resister(0.15) at the output. Now it seems the output voltage(1.32V) is lower what we set(8.4V) through I2C, could you help to check?
The register setting is listed below:
0x12 0x0030 (option register)
0x14 0x0c00(charge current)
0x15 0x20c0(charge voltage)
0x3f 0x1000(input current)
BTW, I have jumped the pin CMSRC to VCC input(9V25), but I don’t know why I need to do that, because in the block diagram, this pin provides the base power for the voltage pumper of ACDRV.
Please check the schematic below:
And I have tried to switch the sense resistor back to 10m. I can see some voltage output there. But it seems that the charge current I set through I2C is not accurate. Please check the voltage I measured across the load resistor(36ohm) at the output:
|
charge voltage register setting: 0x20d0
|
|||||||||||||||||
This is a bit confusing.
Thanks so much!
Best Regards,