Dear Power Experts,
On the LM2738YMY switching regulator part the absolute maximum voltage listed for the feedback pin is 3V.
-
Is this truly a voltage limit not to exceed on the pin or is it to keep the current flowing into the pin at a non-destructive limit?
-
If the current is limited by the top resistor in the feedback network could the part survive if the current was limited below a certain level?
-
This technique can be used on some circuits since the ESD structure attached to the pin can bleed away a small current without being damaged.