Hi TI support members.
I'm Chiaki Endo.
Our question has been asked by Mr. Kanao of TI Japan until now.
Please confirm below items.
1.When full charged and continue charging, the battery will not recharge unless it reaches "Recharge Threshold".
Does the SOC of GG fall below 100% during that period?
We worry that SOC value will be changing from 100% to 99% or 98% after full charged and continue charging.
If it is, what is suggeston to avoid it?
We worry that SOC value will be changing from 100% to 99% or 98% after full charged and continue charging.
If it is, what is suggeston to avoid it?
2.Does the INT output at BAT_FAULT(OVP) transmit 256 us pulses only at the moment when BATOVP (VBAT_REG * 104%) is exceeded?
or continue to deliver 256 μs pulses at regular intervals while exceeding it?
And how much is the response time for sending INT with OVP?
Best regards, Chiaki Endo