Part Number: LM317
Other Parts Discussed in Thread: LM337, TPS7A33
My application is to post regulate an SMPS output with +5V and -5V.
Is it ok to use LM317 where the input is floating, and the output is nailed to ground. A picture will make this clear.
This is the normal way to connect up the LDO. Vbat- connects to ground and Vbat+ connects to LM317 input. Vout+ is a positive voltage relative to ground. Okay.
Now consider this alternative. The input battery is floating, so just connect the LM317.OUT to GND and use the Vbat- as the output. I think this works, just not sure how good.
In my case, Vbat is the floating output of an SMPS supply.
I am considering this because the negative LDO LM337, has crummy frequency response as compared with the LM317.
Any thoughts?
gene