This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 112
Part Number: TPS7A54-Q1
Please clarify the connection of the Bias pin when not used (Vin = 5.5V, Vo = 5V)
The Pin table states that "A 10uF capacitor or larger must be connected between this pin and ground" it also states the pin must be left floating or tied to ground if not used. The EVM has the pin floating and a 10uF cap to ground.
What is the correct configuration?