Hi team,
if the input impedance is larger, why it still needs to be much less than 100kohm?
What's the meaning of much less than 100kohm? 10kohm or 1kohm, or 50kohm which ones are less than 100kohm?
If we use a larger resistor here, for example 400kohm, what's the risks here?
Thanks.