Hello,
I want to use TPSM846C32 for Xilinx Zynq FPGA (XCZU4CG).
The datasheet of power module says: the minimum required output capacitance network consists of four 47-μF (or two 100μF) ceramic capacitors plus two 470-μF.
On the Zynq side, I have numerous rails (VCCINT, VCCINT_IO, VCCBRAM, ...), each requiring proper decoupling capacitors, that I consolidated into one 0.85V rail.
My question is, if the caps required by FPGA, exceed numbers required by TPSM, do I need to have both caps required by TPSM and FPGA or can I treat them as one capacitance?
If so, does this depend on the distance between TPSM and load? In my case the distance is small - TPSM will be adjacent to FPGA.
I googled a bit but didn't find anything conclusive.
Thank you for your help.
Kind regards,
Karol