ist it possibel to get a Schematic review
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dieter,
The charger TS pin is used to stop charging outside of a certain temperature window typically 0-45C. If you have a gauge that can communicate that information and disable the charger, then the charger TS pin is not needed. To disable the charger TS function, you will need to add a resistor divider that sets the TS voltage in between the VLTF (73.5% typical of VVREF) and VHTF (47.2% typical of VVREF).
Regards,
Jeff