We have made battery sharing circuit /PCB using BQ24133. it primary functionality looks ok. The Li-on battery is getting charged . But it takes 8-9 hours for full charge. it is consuming only 300mA.. Can anyone help me how to increase the battery charging current ( our expected charging time for full charge is 3-4 hrs).
the measured values are
voltage at ACSET pin is 0.807V
ISET voltage is 0.404V
As per design,
Input ACSET voltage is 2A
I charge is 1 A
Thanks in advance for your reply.