Other Parts Discussed in Thread: UC1708
Hello
In my circuit, I use UC1708-SP driver. I added my schematic.
INPUT pin characteristic of UC1708-SP is really interesting. UC1708-SP IN pin behaves like a voltage divider from its isolated supply and some capacitance inside.
I also couldn't understand ENABLE pin characteristic.However, it works properly as schematic.
The block diagram in datasheet is insufficient to understand the input characteristic.
Attached schematic works however, circuit is sensitive and the power consumption from isolated supply is higher than 5W. However, there is just 20C temp. rise on UC1708-SP which is normal I think.
Could you please;
*please review design
*please explain INPUT pin characteristic
*please explain why there is a need 910R from INPUT to ISO.SGND. When I use higher than 910R at INPUT pin, in condition of PWM goes continously low, INPUT pin detects PWM signal as high and turns on MOSFET. (Circuit works reversely.)
*please explain why the series resistance 8.2R is good for INPUT pin, higher than 47R the driver signal is very bad and converter doesn't work properly.
*please explain what is the reason of high power consumption maybe the system is damped on 910R or 8.2R.
*Please, offer interface for INPUT pin for isolated PWM supply.
Thank you.