Hi sir
pls help check above questions,tks!
(1)11 pin :COMP pin voltage and load current relationship? Is Positive correlation or negative correlation when the COMP voltage stable ?
(2)What is the maximum value of CSP voltage? After the CSP voltage reaches a certain voltage value, will it trigger the overcurrent protection function of the IC?
(3)In the datasheet, when using the interleaved BOOST circuit, the sub-channel FB pin is connected to VCC to connect to the VCC pin of the IC or to a high level. If the high level is connected, what is the voltage requirement?