Currently we are facing the failure of the PFC MOSFETs in out product and the PFC is controlled by UCC28180D. More details are provided below…
We understood PFC control IC as one of the main cause, Need your support here…
Details:
Design: 230V AC to 650V DC BOOST PFC Converter
Failure Happens during the Step load of 3kW at the output… (Load Transient)
Waveform-1 during the MOSFET failure: (Yellow: Input Current, Blue: DC BUS/output voltage, Red: Inductor Current, green: MOSFET Duty)
We did more experiments to understand what is happening to the control… we had some observations with PFC current sense changes…PFC Current sense in the Design is 7.5mohm
PFC _with Load Step_2kW_with15mohm
PFC _with Load Step_2kW_with7.5mohm
Found that duty is clamped at the peak of input with higher causing current increase between 60 to 120 deg. and current shape is becoming non-sinusoidal.. below is the comparison waveform with 15moh and 7.5mohm Current sense
Kindly help to understand this better and resolve the issue ASAP.
Regards
Siva Tella