Other Parts Discussed in Thread: BQ24192
Hi TI guys,
I wondered of if you can shed light on a couple of questions regarding problems I have. Firstly, can you explain what the difference is between the BQ24192 and BQ24192I. From what I can see reading the data sheet, it's the default values being different and the pre-charge current on the BQ24192I is limited to 640mA max. Other than that, can I assume that the BQ24192I can be configured to deliver a charge current of up to 4.5A?
OK so here is my main issue. I am using the BQ24192I in a configuration as per the application note design within the datasheet whereby the input ILIM is set externally to limit to 3A (177R) as is the charge control register. I have disabled the watchdog for now, so custom I2C settings do not revert back to defaults. The input source is an adapter capable of delivering 4A @ 5V, so this I feel is more than adequate, however, if the batteries (Li-ion single cell 4 in parallel, totalling 13,400mAh) are taken down to just below 3V, say 2.9V, and a charge cycle is started, once over pre-charge, the maximum current seems to be 1.7A. Why is this when everything indicates settings wise that it should charge at 4A
This is what I write to the registers via I2C on power up:
REG 05 = default value & b11001111 - Disable watchdog
REG 04 = b10110001 - Set charge voltage to 4.208V
REG 02 = b11100000 - 4.096A
REG 00 = b00111111 - 3A
REG 06 = b10110111 - 50mOhm as there is a series Isense resistor for fuel gauge, VClamp to 80mV and Thermal regulation to 120deg. C. (Tried this left as default, didn't make much difference)
REG 03 = b00110011 - 512mA pre-charge and termination current.
I'm monitoring the thermal regulation bit (1) in REG 08 and this is not being set.
Please can you help as I'm out of ideas!
Many thanks.