Part Number: BQ25895
I have a BC25895 that is only charging a 1S Li-Ion 2020 mAh battery at around 200-350mA. The data from the registers show that it knows the input current limit is 3.25 A, the fast charge current limit is 2.048 A, and it is in the fast charge part of the charging cycle. After enabling the conversion ADC, I was able to read that the charge current is only 0.2A. This was confirmed with an external DMM measurement. The IINDPM Status bit is 1, which means it thinks it's drawing too much current from VBUS on the USB input. However, the supply I'm using shows that in total only 350mA is being sourced (150 mA for the rest of the system, 200 mA charging the battery). Charging current increases to 350mA when the rest of the system is turned off. I've seen this total go to 450mA sometimes, but never over 500mA.
The circuit is the same as Figure 47 in the datasheet, except that there is an 8A fuse in series with the battery.
Here's a dump of the register data I'm reading.
| REG | Hex |
| 00 | 7F |
| 01 | 05 |
| 02 | 3D |
| 03 | 3A |
| 04 | 20 |
| 05 | 13 |
| 06 | 5E |
| 07 | 9D |
| 08 | 03 |
| 09 | 44 |
| 0A | 93 |
| 0B | 76 |
| 0C | 80 |
| 0D | 17 |
| 0E | 53 |
| 0F | 53 |
| 10 | 4F |
| 11 | 98 |
| 12 | 04 |
| 13 | 46 |
| 14 | 79 |
Blue values are read after turning on the internal ADC and waiting at least one second.
I've been simulating a USB DCP by connecting a bench supply at 5V and 2.5A to the Vbus pin, and then shorting the D+/D- lines, as per the BC1.2 spec. The detection cycle looks like this:
Top trace is USB Vbus, bottom two traces are D+/D-. I can see the primary and secondary detection happening on D+/D- in the first 0.6V bump, and then it goes to 3.5V upon detecting a DCP as per the BC1.2 spec. However, I'm only guessing that the long period of 0.6V again after that and the return to 3.6V are part of the Adjustable High Voltage Handshake. In any case, the register data shows that it successfully detected a DCP with the proper current limit. The noisy part at the end was when I plugged in the battery.
Why does it think it needs to limit charge current to 200mA when it knows the max input current is 3.25A, max charge current is 2A, and the rest of the system is only drawing 150mA? Is the internal input current sense circuitry broken?