This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3843A: UC3843A

Part Number: UC3843A

Dear Sir,

I am facing issue while designing DC to DC converter using device UC3843A.

Input Voltage- 18V Dc to 60V Dc

Required output- 12V Dc.

Required Current- 0.5A.

Issue:- Not able to perform load regulation.

please help on this.

Regards,

Karan.