Hi,
We got a question from customer about LM5161-Q1.
Could you help us?
[Question]
How much is the recommended minimum switching frequency under the following condition?
Topology: Fly-Buck-Boost
Vin=5~20V
Vpri=-8V
Ipri=0A
Vsec1=15V
Isec1=50mA
Vsec2=8V
Isec2=100mA
They are considering 100kHz switching frequency. Therefore they would like to know the recommended maximum on time and Ron.
Best Regards,
tateo