Part Number: BQ76940
Dear TI team and forum members,
how do I calculate the voltage value from the "Battery Voltage" ADC raw value of the bq769x0 chip. I was able to calculate the cell voltages successfully, but I can't get any further with the battery voltage. I am aware that the delivered value is a sum of the cell voltages, but I would have to transfer fewer bytes if I could interpret the value correctly, which saves time and traffic on the bus.
Unfortunately, the only section in the documentation on this subject is incomplete. Please see the attached screenshots.
RAW 0x8F50 -> 36688 in decimal so what are the unknown factors? Also the ADC Gain and ADC Offset doesn't seem to be the answer.
Thank you in advance!
MaBo