Hi,
I'm developing a BT Power device and I want to use the TP2372-4. I'm trying to make compaltible our product with complaint injectors and non complaint injector. I'm having problems to figure out how to make the BT power device compatible PoH PSEs and with IEEE802.3af/at/bt injectors at the same time. My power device needs to be clasified as class 6 ( it needs 42w at the PD), but if I set my PD as Class 6 it won't be powered up by a PoH ( which can just interoperate with Class 4 or less). I could place a switch to change the CLSB between Class 6 and Class 4 but I would like to avoid that solution as it relays on end user doing somehting. Is there any way that I could detect the injector being a PoH and change automatically from Class 6 to Class 4?, or any otehr solution that I could use?.
Thanks in advance,
Daniel.