This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25630-1EVM-291: EVM issue

Part Number: UCC25630-1EVM-291

Hi Team,

Here are some issue happened while testing with UCC25630EVM:

1. When output load form 0A to 10A, output voltage drop from 12V to 0V, then recovery.

2 After output current increase to 14.5A, EVM goes to over current protection, wait a while(about 5 sec) then adjust output current to 10A, the output didn't recovery, have to decrease output current down to 0.0xA, then output voltage get recovery.

Could you please help on this case?

Thank you.