Hello,
I'm trying to understand what "factory configured" means exactly. I'm trying to design a single cell protection circuit and the data sheet says the Vovp, Vuvp, Voc, and Vscd are all factory configured. I'm wondering what would be the typical setting coming out of the factory would be? I'm trying to limit my charge and discharge to 2A, short circuit detection is flexible, and want to protect the battery from an over voltage of 4.2 V and under voltage of 2.8 V. I expect I simply just change my shunt resistor to accommodate the current protection setting, but what do I change to accommodate the over and under voltage? Or can I specifically ask for the settings from the factory?
Thanks,
-Kris