This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS770: Higher voltage alternatives

Part Number: TPS770
Other Parts Discussed in Thread: LP2951

I am using the following regulators and need to increase the input voltage to 12V.  I would like to use the same package and Enable Pin is Active LOW.   Can you recommend a 12Vin capable part?

Part #1: TPS77033DBVR

Part #2: TPS77001DBVR

 

 

  • Hi David,

    Unfortunately we do not have very many linear regulators that enable the output with the enable pin tied to GND. None of the 12 V devices in the SOT-23 package have an enable pin with this logic. Although not in the same package, please consider LP2951.

    Very Respectfully,
    Ryan