Other Parts Discussed in Thread: BQ25700
hi
About BQ25700 charge current issues:
VIN=12V; set charge voltage 13200mV, REGN=5.99V; cell_batpresz=3.48V, 58%-3cells;
issue1: when VBAT<7.2V start charge, charge current oscillated;
issue2: in CV mode, charge current oscillated, much bigger than you test on DB 30mmA ripple, how to decreas?
issue3: the same with light load, CV mode charge switch to OTG mode, the current ripple is big different, how to explain?
0x12[10]=1, set minimum PFM burst frequency to above 25kHz to avoid audio noise, will be valid for charge and OTG mode?
look forward you Answer ASAP.
Thanks
BR
JellyBQ25700 current.docx