Other Parts Discussed in Thread: TPS63070,
hi,
I need to verify my design, that i'm working on, A Remote WSN node which will be powered by a Renewable Energy Source like Solar, and the Solar Panel Specs are as follows
Vmp=+6v
VOC=+11V
Imp=0.5A
Pmax=3.5W
I have selected BQ2601 as the charger IC for my Li+ion Battery 18650 type, requirements are mostly met with ours, And a Boost convertor like TPS63070 is used to power other sensors
Which will work at greater than +3.3V, I'm very keen to know that, Is this the Best approach of mine?, Or any Best practices are suggestible which can be adopted into my design.Schematic_For-Eval_Sheet-1_20190314114451.pdf