Part Number: UCC28950
Other Parts Discussed in Thread: UCC28951
I'm working on a project that contains a 5KW DC/DC converter.
I’m making some design calculations based on datasheet (SLUSA16D) formulas and I have some questions.
1. P. 40. eq. 30 for magnetizing inductance it seems must be just Dtyp not (1-Dtyp), is it correct? In another formula below (P. 50 eq. 108) it's only D in the same equation. And the formula for minimum magnetizing inductance taken from another source says L> (n*D*Vin) / (4*I*f)
www.researchgate.net/.../320490239_Design_Of_a_50_kW_Phase-Shifted_Full-Bridge_Converter_Used_For_Fast_Charging_Applications eq. 6
2. Why in this formula (P. 40. eq. 30) do we take only one half of output pulsing current dILout*0.5?
3. My converter works as "step up", it converts from low (~24V) to high (400V). So I'dont need synchronous rectification on secondary as currents relatively small. I'm planning to use simple transformer with one winding on secondary side with simple diode bridge rectification. Can I use controller this way?
Could someone answer these questions?