Other Parts Discussed in Thread: LM36274, TPS61042
Quick question concerning the LM36923H and LM36274 modes of operational:
- Is there a way to preprogram a current for every LED out
- Can you separately turn ON/OFF every LED out at any moment with preprogrammed current
- Can I not connect and not use the LCM driver for the LM36274
from a control perspective, the desire is to control this with I2C.
If there is a better part to recommend for the above objectives, see design parameters:
VIN range: 2V-3V
Vout: 6.5V max – single UV LED (per channel)
Iout: 50mA max per channel