1) Is there any way to get temperature out of the chip?
2) When we turn a ENABLE off it takes the chip 40-50uS to stop output switching, is there something we can do to speed this up? INFO - we are making a power supply for an FPGA that needs sequencing which is done with a PIC uContoller. We have 3 shutdown modes, a standard shutdown controlled by the PIC, a FAULT shutdown (all supplies shut down at the same time, are pulled to ground with FETs, using the chip CE line, in case of any supply overvoltage, this works great by the way, no CE delay to output), and a FAST sequenced shutdown, in case we loose battery. This is controlled by the PIC by a fast de-sequencing using the ENABLE lines and we are shorting the output of the supply to ground with our pull down FETs for 40-50uS until the chip stops switching.